AXIS#.IL.OFFSET
Description
This value is added to the overall current loop feedforward value. A constant current command can be used to compensate for gravity.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
A |
Range |
|
Default Value |
0 A |
Data Type |
Float |
See Also |
AXIS#.IL.FF |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.IL.OFFSET | 0x500A | 0x10 | DINT | 1000:1 | - | RW | False |
AXIS2.IL.OFFSET | 0x510A | 0x10 | DINT | 1000:1 | - | RW | False |